Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPICE MODEL FOR STB57N65M5

Hi,I am designing a 500W PFC and am considering this part as the main switch. I would like to try and model losses for this part and a SPICE model would be useful.Also any suggestions for a good part would be appreciated,Thanks

willnick by Associate
  • 787 Views
  • 0 replies
  • 0 kudos

Resolved! Solar charging and autonomous power supply for MCU

Hi All,I'd like to create a PCB for my school project that captures energy from a small solar panel using SP1040. The harvested energy will then be used to charge a LiFePO4 battery (3.6~3.7V) through the LD6924 battery charger. Additionally, the volt...

Schematics.png
Levan by Associate III
  • 4620 Views
  • 3 replies
  • 2 kudos

Resolved! How to stop RF activity on STM32WB55RG

I am using Zigbee wireless communication using STM32WB55RG. I would like to reduce the current consumption to 1μA after it has finished its role, but the current does not go down. What should I do now

Born2 by Associate II
  • 1506 Views
  • 1 replies
  • 0 kudos

Resolved! component identification "st bek p420"

Hi, On a power electronic board I have this component "ST BEK P420" in parallel with the power input. I think it's a costant current regulator. I need a spare part or at least its datasheet in order to adapt another component. I hope you can help me....

EnzoCA by Associate
  • 1501 Views
  • 1 replies
  • 1 kudos

Resolved! Can I directly connect L6824D battery charger output to MCU VBat?

Hi all,I'm interested in utilizing a solar cell as the power source for my MCU project. To achieve this, I've implemented a power harvester that, in turn, employs the L6924D battery charger to efficiently charge a lithium battery. I'm seeking guidanc...

Levan by Associate III
  • 1819 Views
  • 2 replies
  • 1 kudos

Topology selection

Hi TeamMy Design inputs:input voltage range 1:- Vin min:316 Vdc, Vin nominal:587Vdc, Vin Max: 815Vdcinput voltage range 2:- Vin min:417 Vdc, Vin nominal:700Vdc, Vin Max: 1000Vdcinput voltage range 3:- Vin min:417Vdc, Vin nominal:800Vdc, Vin Max: 1200...

VND5050JTR-E channels in parallel ?

Hi,I'm need a high side switch ( 24V/10A ) and was thinking about the VND5050JTR-E, but in order to avoid junction overheating, I'd need to split my current between the 2 channels. Does anything in the chip prevents me to to do this safely ?Best rega...

SDW_YMo by Associate
  • 545 Views
  • 0 replies
  • 0 kudos

GUI L99615C Software issue

Hello,I have a problem with connection L99615 with dedicated software STSW-L99615C. First of all, there is no automatic connection to the com port (I read that it is possible, so I made it manually but it still looks strange - one time I saw that my ...

jojoanaa by Associate
  • 1058 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.