Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

(STC3115) Effect of battery discharge on OCV measurement

How much error will occur in the SOC calculation results if discharge occurs during the initial OCV measurement?Also, is the OCV measurement timing other than the initial stage of charging? At that time, are you looking at the battery current and mea...

ddddumi by Associate
  • 899 Views
  • 0 replies
  • 0 kudos

Resolved! STBC15 output current?

Hi all,I recently stumbled upon STBC15 and I am interested in integrating it into our next design. However, I am lacking a critical parameter from the datasheet: what is the typical and maximum allowed current flowing from VBAT to the OUT pin?

icharala by Associate II
  • 1436 Views
  • 4 replies
  • 0 kudos

STTH30RQ06D 2K

We would like to check if we can get the support of STTH30RQ06DY 2k ? Please feedback.

Getting started with the STEVAL-WBC86TX Evaluation board

I am trying to communicate to the eval. board using the WPSTUDIO GUI, however I am unable to connect. The board uses an FTDI FT260Q that communicates through HID Interface and does not require any additional drivers; however I am still unable to conn...

Farkha by Associate
  • 1125 Views
  • 1 replies
  • 0 kudos

Resolved! Low side switch

Hi,I need low side switch which is Automotive qualified, support more than 60V with over current protection feature. Please suggest some parts which meet followed requirements. Please reply as soon as possible. Regards,Sangeeta K

T810-600B-TR TRIAC Not Turning ON With Load

I have a legacy project that I converted to an SMT design but the existing TRIAC is not meeting all specifications of the product. I am evaluating other options and one option that I'm looking at is the T810-600B-TR. In this application, the transist...

PDIhawk by Associate III
  • 14755 Views
  • 14 replies
  • 0 kudos

Resolved! RCD Snubber

I'm designing a automatic fan switch using a BTA26-800CWRG triac.  I'm planning on a RCD snubber.  All I've seen so far show a single diode across the resistor of the snubber.  But it seems if the snubber is snubbing an AC source there should be two ...

RodB by Associate
  • 2269 Views
  • 1 replies
  • 0 kudos

IPower management IC STPMIC1APQR

 I am using the power IC STPMIC1APGR to manage the power for my circuit boardCurrently I can't connect to STPMIC1 1.07 software (I use win 11 and USB to I2C converter CH341T_V3)my diagramThe software is not connected yetUSB to I2C

Screenshot 2024-01-07 162320.png Screenshot 2024-01-07 162429.png Screenshot 2024-01-07 162520.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.