Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Testing workflow for structural reliability?

Hello everyone,We are currently working on structural validation and material testing workflows.Has anyone here implemented automated reliability testing setups?We documented some testing methods and validation ideas here:Would love to hear your feed...

fauzia by Associate
  • 166 Views
  • 0 replies
  • 0 kudos

STGAP2D pin8 N.C. explain?

Hi . I'm using STGAP2D SO-14 IC in custom project with custom board , and in datasheet i see pin8 specified as N.C. (not connected). Pin8 must be left floating for ic to function properly , or can it be connected to nearby pin7 (GND) ?  Is this pin i...

ximikas by Associate
  • 194 Views
  • 2 replies
  • 0 kudos

Resolved! L6206Q - SENSE resistors required or not?

The L6206Q datasheet Figure 14 "Typical Application" does not show the use of any additional SENSE_A or SENSE_B resistors connected to pins 45/46 & 15/16 respectively.  Section 4.3 talks about "the external current sense resistor normally used [being...

wnm4 by Associate
  • 268 Views
  • 2 replies
  • 1 kudos

Resolved! Simulation model of L6491

For the analysis and working of the gate driver L6491, we need the simulation model of the gate driver L6491 of LTspice or Pspice. Please provide the simulation model as soon as possible. It would be very helpful to us.Thank you!

Resolved! STEVAL-KITXCB SD pin question

In STEVAL-KITXCB for controlling SD/OD pin of L6491 using such method. PWM_en connected to MCU pin. I want use same principle in my design. Can anybody describe how program this.Is such hw connection support both function for enable PWM and for contr...

Без імені.png
Kuzma30 by Associate II
  • 419 Views
  • 7 replies
  • 0 kudos

Resolved! STWLC89 application related

Hi,Since we haven’t received the datasheet yet, we’d like to confirm the following information:If the receiver side (RX) uses the STWLC89 15 W solution, what is the corresponding 15 W transmitter (TX) model?Which Qi standards are supported by STWLC89...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.