Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

eDesignSuite Transformer

Hello I tried to design a 3-output AC-DC converter using the eDesignSuite. But the software only provides the turns ratio for the transformer and no core suggestions or what so ever was shown.I don't get the idea behind the eDesignSuite software that...

info23 by Associate
  • 193 Views
  • 0 replies
  • 0 kudos

Resolved! Three phase capacitive power supply transformerless

I need to use in our application three phase power supply any of the two phase present power supply should work or with respect neutral also work if any of one phase present.  required for voltage monitoring three phase or sequence detector. any refe...

Glodhi by Associate II
  • 170 Views
  • 1 replies
  • 1 kudos

VNQ9080AJ Flyback diodes for inductive loads

Hi,I'm designing a custom PCB and I'll be using a VNQ9080AJ to drive 4 inductive loads (hydraulic valve spools).Is the protection diode in the datasheet sufficient for that application?The device will drive up to 28 VDC ~3.5 to 5 amps inductive loads...

emachabeeinnotag_0-1769613302763.png

EVAL-L9963E not configured

When configuring the system, firmware version 1.6 is detected correctly. However, when the configuration ID is set to 1 as mentioned in the manual, it is not acknowledged by the device (shown in red).

Keyur0036_0-1769485983734.png

Resolved! Does "MJD31CT4" meet UL94 V-0 rating?

Hi, I'm checking the flammability specifications for MJD31CT4. I need to know if the molding material of this part is rated UL94 V-0. If it's not V-0, could you tell me what the official rating is? Any link to a supporting document would be much appr...

kwak by Associate
  • 295 Views
  • 1 replies
  • 0 kudos

L6981(C50DR) dies on hard switching of input power

Hello everybody,I'm using an L6981C50DR for supplying a small board with 5V. The schematics is attached and should be perfectly conform to what is described in the specification from https://www.st.com/resource/en/datasheet/l6981.pdf as "Figure 4. Ba...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.