2026-02-17 3:13 PM
The L6206Q datasheet Figure 14 "Typical Application" does not show the use of any additional SENSE_A or SENSE_B resistors connected to pins 45/46 & 15/16 respectively. Section 4.3 talks about "the external current sense resistor normally used [being] eliminated." AN1762 in section 3.5, discusses the selection of sense resistors and suggests that they might be part of the over-current setting process (which the datasheet suggests is handled entirely by the R_CL resistors).
So which is correct? Datasheet or AN? Are sense resistors required or not? If they are required, how are they selected and how does that selection work with the selection of R_CL current limit resistors?
Solved! Go to Solution.
2026-02-18 3:49 AM
Welcome @wnm4, to the community!
You have allowed yourself to be confused by two fundamental differences:
So whether sense resistors should be used depends on your application and requirements. If you want to use them, you will find calculation notes in the AN1762 mentioned above, section 3.5, for example.
Does it answer your questions?
Regards
/Peter
2026-02-18 3:49 AM
Welcome @wnm4, to the community!
You have allowed yourself to be confused by two fundamental differences:
So whether sense resistors should be used depends on your application and requirements. If you want to use them, you will find calculation notes in the AN1762 mentioned above, section 3.5, for example.
Does it answer your questions?
Regards
/Peter
2026-02-18 7:05 AM
Thank you Peter, this does indeed answer my question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.