2026-02-21 10:32 PM
Hi,
We are designing a compact, battery-powered system that requires a regulated high-voltage DC output with the following specifications:
• Input: 5V
• Output: Adjustable 400V to 1000V
• Load current: 1µA to 200µA
• Very low ripple and noise
• High efficiency and small form factor
The supply will be used as a bias source for sensitive detectors (e.g., APD/PMT-type devices), so output stability and low noise are critical. The output must remain stable across the specified load range.
I am currently considering a closed-loop flyback topology with post-filtering, but I am open to alternative architectures.
Could you please recommend:
• Suitable controller ICs from your portfolio?
• Relevant reference designs or evaluation boards?
• Design techniques for minimizing ripple and noise at these voltage levels?
Any guidance or application notes would be greatly appreciated.
Thank you.
Solved! Go to Solution.
2026-02-24 2:41 AM
This application note by the late, great Jim Williams might be of some interest to you:
2026-02-23 12:33 AM
In principle, this can be done with a flyback, but the effort required in relation to the output power is probably too great and a flyback would be significantly oversized. You should therefore consider something that has been used for many decades to generate high voltages with low output currents: a voltage multiplier, i.e. something similar to a Cockcroft-Walton generator. With 12..13 stages, you should achieve 1kV with some control reserve; 15...22nF capacitors should be sufficient.
Advantages:
Disadvantages:
You should urgently observe the usual precautions to minimise ripple and noise:
There are a few devices in the portfolio of STMicroelectronics that you can use in such a voltage multiplier:
Hope that helps?
Regards
/Peter
2026-02-24 2:41 AM
This application note by the late, great Jim Williams might be of some interest to you:
2026-02-25 1:01 AM
Thanks Peter for the answer its helpful.
2026-02-25 1:01 AM
Thanks. this is exactly what i was looking for.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.