I am looking for L7815ABD2T MTTF value
hello:I am looking for L7815ABD2T's MTTF value,Can provide me with this document? the Part No. :L7815ABD2T
Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
hello:I am looking for L7815ABD2T's MTTF value,Can provide me with this document? the Part No. :L7815ABD2T
Hello STmicro Team, I have done a propagation delay analysis using VNL5030J-E. The Delay-on time, rise time and delay-off time does not matches with the datasheet Values. Please check and let me know your feedback in this. I am attaching here the sna...
Request any history on PCN for the L7905CD2T
I am trying to get the spice model for STW3N170 MOSFET, it does not seem to be with the other info for the devive.Any help appreciated. Paul
Hi,We are using STPM32 with LPC controller, when observing the startup reset pulse we are getting as in the picture attached. Both SYN and SCS pins are initialized high but when powered on SYN is coming low for some time then it is taking 35ms delay ...
Hello, I am having a problem with a design using the ST8R00WPUR.The input is 5v, the output is 10.5v, the load is 22 ohms (477mA).The problem is that the output drops below 3v for 200ms when the load is applied, before returning to 10.5v. The problem...
Recently started working on the L9026 Device, as an initial setup, trying to read the Device ID. With The L9026 Evaluation board Device ID is read as 0x55, With L9026 Placed on the Our Target Board, Device ID is read as 0x56, Was surprised with t...
Dear ST Community Member,Currently working on development of 1.2kW EV Charger. The L6599AD (high-voltage resonant controller) IC is used for half-bridge LLC topology. We have tested the IC separately by giving different voltages at various pins of th...
I would like to know the working principle of the charger bump for MH98, as well as the working principles of CPOUT, CP1, and CP2. Why can the voltage of the bootstrap capacitor reach 11.3V when VDH = 6V? In other words, why can the voltage of CP rea...
Hi all. The data sheet for the LDL212PUR low dropout linear regulator does nor specify the quality of the input and output bypass capacitors with regard to ESR or loss tangent requirements. Most LDO regulators require at least one low ESR bypass cap...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.