Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VN7050AJ SEL0/1 unused pin state

Hello all, in whole datasheet for VN7050AJ is not mention about default state of pins SEL0 and SEL1, but there is information that those pins can be left unconnected. Is there an internal pull-down resistor which selects current sense for CS output? ...

Eiffel by Senior
  • 696 Views
  • 0 replies
  • 0 kudos

Resolved! CCIC1I Datasheet with ST LOGO

Hello STMicroelectronics Community,I'm reaching out to you with a question regarding an SMD IC bearing the ST logo. I am in search of the datasheet for the IC labeled CCIC1I in the TSSOP28 package. Unfortunately, I couldn't find any information about...

Resolved! Isolated 10V power supply using viper222LSTR IC

Hi ST team,I have design the 10V isolated power supply design using viper222LSTR IC having universal input AC supply. Schematic of the circuit is attached here.When i am increasing the input voltage, voltage across the capacitor C7 maintain constant ...

Pemendra_1-1713170439634.png
Pemendra by Associate II
  • 2255 Views
  • 3 replies
  • 1 kudos

L6599AD eDesignSuite

我想为 L6599AD 设计 LLC 参数,但我找不到设计工具。在 eDesignSuite 上未找到任何设计条目。你能告诉我这是哪个参数设计工具吗?

andyqin by Associate
  • 870 Views
  • 0 replies
  • 0 kudos

Searching for BTA06-600CRG SGS report, I am in https://ols.st.com/s/ no find

你好!我正在寻找 BTA06-600CRG SGS 报告,https://ols.st.com/s/ 我没有找到任何要下载的文件。我可以在哪里申请?Message translated to English:  Hello! I am looking for BTA06-600CRG SGS report, https://ols.st.com/s/ I didn't find any file to download. Where can I apply for it?

GuGu by Associate
  • 819 Views
  • 2 replies
  • 0 kudos

Resolved! Output power of device vs it's evaluation board

Hi Looking at the PD55015 it has a declared output power of 15W. The evaluation board STEVAL-TDR016V1 on the other hand is rated at 30W output power? How can the evaluation boar be rated at twice the output power of the device it is demonstrating wit...

Power over Ethernet to 12V USB-C PD

I’m trying to find a solution to create a PoE to 12V USB-C power delivery adapter as I can’t find one on the market. There are PoE to 5V USB-C PD ones, and PoE to 12V barrel plug ones, but nothing as far as I can tell that will provide the negotiatio...

Resolved! IC TH2008-01

Hi, everybody. I am repairing a machine that uses the IC TH2008-01 from STMicroelectronics, but I need the data sheet. Can you please send it to me? Thank you.

fh by Associate II
  • 1952 Views
  • 4 replies
  • 0 kudos

Resolved! How to configure the STEVAL-WLC38RX board to receive 5W power

Hello everyone!I would like to ask you for some advice on how to configure the STEVAL-WLC38RX board in the WPSTUDIO GUI so that it receives 5W power.The STEVAL-WLC38RX board is placed on the STEVAL-WBC86TX at the distance shown in the photo. I would ...

DZaot1_0-1713881293174.jpeg DZaot1_1-1713881505052.png
DZaot1 by Associate II
  • 2588 Views
  • 3 replies
  • 0 kudos

Resolved! WLC dongle driver issues Unable to load DLL 'HidDongle.dll'

Many customer face dongle driver issues, most because Unable to load DLL 'HidDongle.dll'.  @sjones i post your request in the forum. Key points: This eval board has an on board FT260, which should take care of the I2C to USB (HID) interface without a...

willzhou by ST Employee
  • 3883 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.