Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-IP023 firmware update with STM32CubeProgrammer fail

I tried to update the STEVAL-IP023 board with DFU using  STM32CubeProgrammer, but the STM32CubeProgrammer hang during the procedure, see picture attached.The board is recognized ad DFU device but the procedure does not work.Any suggestion?Thanks 

crudo by Associate II
  • 1200 Views
  • 0 replies
  • 0 kudos

STGF7NB60SL IGBT Material Properties

Dear STM,I am a student and currently working on the lifetime estimation of an IGBT for my research, which involves a Finite-Element simulation on STGF7NB60SL IGBT.To run the simulation, I need to know the material properties of different layers in t...

jsp2 by Associate
  • 665 Views
  • 0 replies
  • 1 kudos

STSPIN958 as a full bridge digital adjustable PSU

Dear all, The STSPIN958 contains all to build a digital controlled (hard switching) full bridge adjustable power supply, including the power mosfets, to my understanding. Or am I missing something important? If set as " Single full-bridge - PWM trimm...

MichiS by Associate
  • 841 Views
  • 0 replies
  • 0 kudos

L6234 Vref capacitor

Posted on April 04, 2013 at 20:26The AN1088 app note states:�Vref ( Voltage Reference).This is the internal 10V voltage reference pin to bias the logic and the low voltage circuitry of the device. A 1mF electrolytic capacitor connected from this pin...

marek23 by Associate
  • 3118 Views
  • 6 replies
  • 1 kudos

STL42P6LLF6

Does STL42P6LLF6  has ST brand logo or Part number on the internal Die wafer ???

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.