Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STGIB20M60TS-L Heating

Hi there!I'm using the STM32G474E-EVAL to drive the STEVAL-IPM20B (eval board for the STGIB20M60TS-L). I'm running my motor (SM3L-084A) at 380V. Note, I've checked with the vendor about running the motor at higher voltage than quoted and there should...

thutch by Associate
  • 872 Views
  • 0 replies
  • 0 kudos

IC L9678 SPI MOSI Frame RID for a Write only register

Hello Team, While going through datasheet, I noticed that there is no mention on what happens if we are trying to put RID for a write only register in MOSI frame. Will it cause any faults or does it work as expected?  

Nixon by Associate
  • 435 Views
  • 0 replies
  • 0 kudos

L9026 Device Configuration Sequence

 Will be looking for a simple sequence to activate the Outputs of the L9026 Note:- INT0 and INT1 are used to activate the chipQuick Response will be greatly appreciated.Thanks,Krishna

Resolved! STWBC86 GPIO for LEDs

Hi,When STWBC86 is operating fully independently without being interfaced with a host system, how can the GPIO be used to drive indicator LEDs to indicate charging status, fault etc? The datasheet shows how these can be programmed to inputs or output...

matt7 by Associate
  • 1549 Views
  • 1 replies
  • 0 kudos

L9305 Daisy Chain SPI

Does anyone know if the L9305 supports Daisy chain communication? 有人知道L9305是否支持菊花链通讯?

YJL by Associate
  • 1454 Views
  • 1 replies
  • 0 kudos

Resolved! L7987 switching frequency

HI Sir,how do we define the switching frequency of the L7987the switching frequency range is between 250KHz and 1.5MHzlooks like if the switching frequency is set to 1.5MHz, the ripple appears to be much smaller, so can we set it to 1.5MHz under norm...

PZha.1 by Associate III
  • 2733 Views
  • 4 replies
  • 0 kudos

Confused about stepper spec & tips on pwm-step/dir

Hello! I have asked the few I know who have knowledge of this and now turn to this one inexhaustible source of knowledge aka. the electronics forum. I was going to buy stepper motors yesterday but got so confused about the spec that I need to get an...

tom22 by Associate
  • 864 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.