cancel
Showing results for 
Search instead for 
Did you mean: 

Can't configure the TCPP01-M12 to 2.5W (500mA)

POLessard
Associate II

Hi,

I have follow the DS12900 Rev 7 Figure 21 (Schematic example for USB Type-C at 2.5W with TCPP01-M12) and still can draw more that 1.5A from USB PD source, the voltage seen on CC1 is close to 1.4V (which corresponds to 3A capability). Not sure what is wrong/missing in the circuit;

POLessard_0-1780418199847.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The 1.4V on CC1 is actually consistent with a 3A Type-C advertisement, so that part does not look wrong.

My main suggestion is to check the USB-PD negotiation and the sink configuration, because the TCPP01-M12 does not limit the load current to 1.5A by itself. It mainly provides CC protection, VBUS OVP, and gate control.

You should check:

  • requested PDO/current in firmware
  • /DB pin state
  • VCC supply
  • whether there is any separate current-limit stage on VBUS

So the likely issue is not the schematic in fig. 21, but rather the system current limiting / PD contract configuration.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The 1.4V on CC1 is actually consistent with a 3A Type-C advertisement, so that part does not look wrong.

My main suggestion is to check the USB-PD negotiation and the sink configuration, because the TCPP01-M12 does not limit the load current to 1.5A by itself. It mainly provides CC protection, VBUS OVP, and gate control.

You should check:

  • requested PDO/current in firmware
  • /DB pin state
  • VCC supply
  • whether there is any separate current-limit stage on VBUS

So the likely issue is not the schematic in fig. 21, but rather the system current limiting / PD contract configuration.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.