2015-04-13 7:36 AM
Hi,
i have a problem with a device that use a STM32F405.Occasionally, after a power off/ power on cycle, the flash (SECTOR 0) are write to zero for the first 48bytes.In the application firmware, there is no procedure that write flash at Sector 0 and the option byte are left to their default values.Any know if there is a problem of flash corruption on the STM32F405 ?!?!Thanks #eeprom #- #flash #stm32f #rewrite2015-04-13 1:55 PM
I've been working with a few STM32F405 parts for a couple years now and have never experienced flash any random flash corruption. However, I don't have any user code that writes to the flash at all. You seem to suggest that maybe you do have code to write to flash, just not at sector 0? A custom bootloader? What toolchain?
2015-04-14 12:28 AM
Exactly Mr. Blinky, I've a custom bootloader (SECTOR.0 + SECTOR.1), several user parameters (SECTOR. 2/3/10/11) and the user application firmware (from Sector 4 to 9..).
The bootloader, which is used for firmware and parameters upgrade, is the only that can write/erase from sector 2 to 11.The application fw can only write/erase to sector 11.No one can acces to the boot sector's for flash write or erase operations.At the beginning of my flash write/erase procedure i've the check of the destination addres, if is not an authorized addres, the procedure return immediatly with a dedicated error. So is very strange found Sector 0 with a different values from the original ones.I saw an event of flash Sect.0 corruption simply after Power Off / Power On cycle.During power off or power on phase, no one (Bootloader and application fw...) acces to the flash for write or erase.As a toolchain i use the yagarto-tools-20121018.The micro is supplied with the 3V3, but in the option byte (...that i left the default values), the BOR is OFF (Vth=1.8V).Do you know if this could create a problem such as flash corruption?!?!Many thanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.