2026-01-25 4:50 AM
hello
I want to use your api to speed up the developpment of a driver based on spi communication, this function seemed appropriate in your stlink-v3-bridge-v1-2-0:
Brg_StatusT Brg::ReadSPI(uint8_t *pBuffer, uint16_t SizeInBytes, uint16_t *pSizeRead)
unfortunatly I found this comment:
* In #SPI_DIRECTION_2LINES_FULLDUPLEX dummy data are sent while receiving.
and i check with a scope that it is the case (data written are '0'),
this is a pity because read/write are frequently simultaneous in spi,
is there a possibility to send data instead of dummy in the mean time we are reading ?
regards
Benjamin
Solved! Go to Solution.
2026-01-25 6:42 AM
thanks for the quick response,
yes I have a FTDI board and software which works as expected, I wanted to use a STLINK instead because the software looked simpler, but it does not come with as many features,
regards
Benjamin
2026-01-25 6:25 AM - edited 2026-01-25 6:55 AM
ReadSPI is a read-only operation. WriteSPI is write-only. There is no two-way read/write operation unfortunately.
This is most likely because the interface mimics the other protocols which are either read or write but not both.
There are some FTDI USB-to-SPI adapters that might work better for you.
2026-01-25 6:42 AM
thanks for the quick response,
yes I have a FTDI board and software which works as expected, I wanted to use a STLINK instead because the software looked simpler, but it does not come with as many features,
regards
Benjamin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.