2021-07-22 1:28 PM
I have compiled some code on the mbed online compiler and copied the binary code onto the mbed Nucleo64 F401RE board. The LED on the ST_Link board starts blinking for a few seconds, and then the binary file disappears from the USB drive. I assume that my code has been flashed, but actually the previous code keeps running, even if I power-cycle the board or press the reset button. This is 100% reproducible. The ST-Link firmware has already been updated with the latest version.
2021-07-22 1:52 PM
> actually the previous code keeps running
How do you know?
Try some "known good" binary, a blinky for example.
JW
2021-07-24 10:55 PM
Hi Jan,
-- exactly that's what I did. I tried the above with a short demo that blinks a simple pattern on the user LED.
Instead the previous blink pattern remains: 3 short LED pulses, 4 long LED pulses alternating.
I suppose this is the original demo program that's installed by ST during production of the board.
Thanks & best regards,
eightbit
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.