2023-07-22 3:11 PM
Hello,
I have been learning using a NUCLEO-F401RE and am now looking to start using a board that I designed that has an STM32F4 chip as well as some other things (e.g., some memory, micro usb) on it.
On the (ubuntu) VM, I have installed usbutils, openocd, and stlink-tools. I
When running "st-info --probe" I was expecting to see details about the STLink on the Nucleo board, but instead received the message "Found 0 stlink programmers".
It seems like the VM is not seeing the usb device as being connected to the STLink (see below), but I don't know how to remedy that.
How can I get the VM to recognize that one of these usb ports is connected to the STLink on the NUCLEO board?
vagrant@vagrant:~$ lsusb
Bus 003 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 002 Device 005: ID 0e0f:0002 VMware, Inc. Virtual USB Hub
Bus 002 Device 004: ID 0e0f:0002 VMware, Inc. Virtual USB Hub
Bus 002 Device 003: ID 0e0f:0006 VMware, Inc. Virtual Keyboard
Bus 002 Device 002: ID 0e0f:0003 VMware, Inc. Virtual Mouse
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Thank you!!!
Solved! Go to Solution.
2023-07-24 4:11 AM
Ah yes, it is a Mac. Can't Fusion manage redirection of host USB devices, like Workstation or Player do?
2023-07-23 4:03 AM
What is your VMware host software? Workstation or Player?
2023-07-23 11:53 AM
Hi Pavel,
It is VMWare Fusion 13 (https://customerconnect.vmware.com/downloads/details?downloadGroup=FUS-1302&productId=1375&rPId=105193).
2023-07-24 4:11 AM
Ah yes, it is a Mac. Can't Fusion manage redirection of host USB devices, like Workstation or Player do?
2023-07-30 9:00 AM
I suspect you are correct - https://docs.vmware.com/en/VMware-Fusion/13/com.vmware.fusion.using.doc/GUID-4819DA9E-3575-4C7F-9912-C2FFBA6CEAD6.html. Thank you for the push in the right direction!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.