2025-03-17 10:25 AM - last edited on 2025-04-16 2:45 AM by Amel NASRI
I’m trying to interface the onboard ISM43362 Wi-Fi module of the STM32BL475 using STM32CubeIDE, but I couldn't find any proper resources or example code online.
2025-03-17 11:42 AM - edited 2025-03-17 11:44 AM
Hello @Shreyu1001
The only available examples to make WiFi work on this board are those WiFi examples.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-17 11:46 AM
but in that theres a common folder which has files... so how do i use it in my project... like pins connections and configurations..
2025-03-17 11:51 AM
@Shreyu1001 wrote:but in that theres a common folder which has files... so how do i use it in my project
I don't understand the problem: all projects are just folders and files - where, exactly, are you stuck?
@Shreyu1001 wrote:like pins connections and configurations..
either do it graphically in CubeMX (standalone, or within CubeIDE), or just write the code.
2025-03-17 11:53 AM
basically i m done with 70 percent project...i just want to send usart1 data which is being printed on teraterm .... to thingspeak api using the on board wifi..... so for that i need to setup wifi... which i m not able to . so need help in setting up wifi module and sending data to thingspeak api ... i m using stm32cubeide..
2025-03-18 1:39 AM - edited 2025-03-18 1:56 AM
So either start with one of the examples projects mentioned by @STTwo-32, or go to the WiFi module manufacturer's website for support
https://www.inventeksys.com/ism4336-m3g-l44-e-embedded-serial-to-wifi-module/
https://www.inventeksys.com/iwin/getting-started-guide/
A quick internet search for "STM32 ISM43362" suggests:
https://github.com/nano256/ISM43362-M3G-L44-Driver
https://github.com/stm32duino/WiFi-ISM43362-M3G-L44
among others ...
@Shreyu1001 wrote:i just (sic) want to send usart1 data
Getting WiFi up & running really isn't a "just" - there's quite a lot to it!
I would strongly recommend that you start this as a separate project - then integrate once it's working.
2025-03-18 3:51 AM
when i try this https://github.com/nano256/ISM43362-M3G-L44-Driver to run and build project . it give me error
2025-03-18 4:22 AM
So fix the error, then!
If you want help to fix the error, you're going to have to describe what, exactly, the error is!
Please see: How to write your question to maximize your chances to find a solution.
You could raise an issue in Git?
2025-03-18 7:11 AM - edited 2025-03-19 7:45 AM
@Shreyu1001 wrote:I try this https://github.com/nano256/ISM43362-M3G-L44-Driver to run and build project . it give me error
@fa31 got it working OK - details here:
PS:
Note that it only works on SPI - not UART:
2025-06-16 6:08 PM
Hi i was wondering if you finally found some documentation or a solution for that
I tried a lot of stuff over the last couple of days but nothing worked
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.