2019-10-24 7:35 AM
For example, I create a new Project (either Matlab 2018a or 2019a using previous STM32mat or latest STM32mat 5.1.0 using cube 4.23 or either cube 5.1.0), Chose for example a STM32F4 discovery board, activate ADC Channels create a new Simulink model and ADC Block)
tic;ADC_Read_callback('Ch1');toc
takes for active channels more than 3 seconds, for inactive channels 0.016 second which would be ok
For a complex System Code Generation takes 5 minutes, most of the time is updaten callbacks of the ADC Registers.
I am doing something wrong or it is normal that it takes so much time?
Many thanks *** nice regards
Jaume
2019-10-25 1:40 AM
Hi @JSerr.441 ,
Yes, you should know that in some cases, mask processing can be slow, especially for very complex Simulink blocks such as TIMERs and ADCs.
There are several reasons we are knowing and you should be informed that I started some optimizations.
Some of these could be included in the next STM32-MAT / TARGET v5.4.0 delivery scheduled for late 2019.
Thanks for your feedback.
Regards.
Cyril.
2019-10-25 3:06 AM
2020-03-24 6:31 AM
Hi @JSerr.441 ,
The STM32-MAT/TARGET V5.6.0 was released in the last days of March 2020.
This release is paired with STM32CubeMx V5.6.0 and with MATLAB R2018b.
This is the consolidation of the previous version V5.4.0 with some enablers for the NUCLEO-H743ZI2.
Regards.
Cyril.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.