2019-08-12 7:45 AM
Hello,
My O.S. is Linux Lite (ubuntu).
I am getting "No such port: '/dev/ttyACM0' msg when I try to open the internal serial monitor in the IDE. I also tried /ttyACM0, etc..
When I use the Aruduino ide I can access the port successfully.
Thanks
2019-08-12 10:02 AM
From your description the problem seems to be related to your Linux system. A quick way to verify this is to short the TXD and RXD serial port pins together, what's called a loopback. Open the serial port and see if the characters you send are echoed back. If not then the problem is not in the STM32 board.
Jack Peacock
2019-08-12 10:07 AM
But I can use a different IDE without a problem, the arduino IDE using the same PORT. I do not have both IDE's open at the same time.
Thanks for responding.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.