Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.
I want to use flash as eeprom by using hal library on stm32l476rg.How can I create the flash_read() and flash_write() functions? (functions will read and write data of type uint32_t)
In order to make the printf function accessible from other libraries, I create a retarget library where I call stdio and write my own implementation of _write function using UART peripheral. So when I want to use printf in another library. I add incl...
Hi All, I'm using a STM32F030x4 that has no EEPROM but I don't want to implement EEPROM emulation on the Main Flash as I only need to 'save' a couple of bytes during power off.Is it possible to use the 'User data option byte' @ 0x1FFF_F804 as a non-v...
I have a project which needs to store the state of the program on an eeprom.Unfortunately there is no built in eeprom on stm32f7508-dk board.I have bought M24LR64 chip for i2c eeprom.Unfortunately the program get crashed on read operation (only when ...
In the example projects there is no dedicated __ARMCC_VERSION (ARM compiler V6).file: stm32_wpan_common.h, in the BleHeartRateRTOS example#if defined ( __CC_ARM ) #if defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6010050U) //We never get here! ...
As shown below the screen, when I am running the MCU application, it is running without any flaws. However, when I notice the TraceExceptions window on Keil IDE, noticed a large number of hard faults occurring. But these faults do not trigger fault h...
Does someone know if system workbench will work also on windows 11? Thanks and regards, Piero
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.