2003-05-19 1:27 PM
Which ST10 type can be insted of C167CS-LM from Infineon?
2003-05-18 8:39 PM
Hello
My customer have designed the automotive project that used C167CS-LM would like to changed to ST10 but didnot know which part no will compatible pin by pin and also want to know the old software used Keil C-Complier still used for ST10 or not? BR's JOM2003-05-19 1:27 PM
There nothing exactly equivalent but is two parts that could be used.
If you need 2 CAN, the ST10F269 will do the job. It has on top of that some built in Flash and a MAC cell. (see enclosed application note) If you want a ROMless device the ST10R167 has one CAN bus only and could do the job. Keil compiler fully support both devices. ________________ Attachments : an1314__compare_C167_F269_.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0KI&d=%2Fa%2F0X0000000bXO%2F6f15WzwJPl14GgLq1KY5GvB2dobJYd82C1o0ieJgGHo&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.