2004-04-24 12:43 PM
2011-05-17 3:00 AM
Hi
I am using the uPSD3212, and planning to have the primary flash as program space and the secondary as the data space. The primary flash is devided in to 4 sector of 16K and I am planning to stack them up from 0x0000 to 0xFFFF. The socondary flash is 16K and I am planning to have it as two banks of 8K each and Please tell me if this will work ok or not?2011-05-17 3:00 AM
Thank You
Maybe I will ask you some more question when I do this. Since you have done it. If you don't mind. Thanks again.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.