2009-06-04 3:20 AM
Unable to set the SCAN bit in ADC_CR2
2011-05-17 6:03 AM
Hi,
We are using the STM8S 128 eval board, RLink debugger and STVD toolset. We are unable to use the ''single scan mode'' of ADC. Setting the SCAN bit of ADC_CR2 doesn't actually set the bit and there is no change in the status. We even tried to modify the register value manually using the Peripheral register's view with STVD and also from the Memory view window. But it just doesn't let us set the SCAN bit. Please let us know if there is any solution for this. Regards, SU2011-05-17 6:03 AM
Hi Sandeep,
The ''Scan mode for single and continuous conversion of a sequence of channels'' feature doesn’t available for the STM8S20xx product if you need this feature you can use STM8S105x product. For more details about the products features availability refer to the products datasheet Regards mozraWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.