2025-09-18 2:27 AM - last edited on 2025-09-18 2:31 AM by Andrew Neil
Dear ST,
I am working with the STHS34PF80 PIR sensor on an i.MX8MP platform, using the upstream-style IIO driver (st_sths34pf80). I am attempting to run the sensor in continuous mode (buffered streaming), but iio_readdev always times out with no samples delivered.
echo 1 > /sys/bus/iio/devices/iio:device3/algo_reset
echo 4 > /sys/bus/iio/devices/iio:device3/lpf
echo 200 > /sys/bus/iio/devices/iio:device3/threshold
echo 50 > /sys/bus/iio/devices/iio:device3/hysteresis
echo 4 > /sys/bus/iio/devices/iio:device3/sampling_frequency
echo 0 > /sys/bus/iio/devices/iio:device3/events/in_temp0_thresh_rising_en
# Enable scan elements
echo 1 > /sys/bus/iio/devices/iio:device3/scan_elements/in_proximity_object_en
echo 1 > /sys/bus/iio/devices/iio:device3/scan_elements/in_timestamp_en
echo 1 > /sys/bus/iio/devices/iio:device3/scan_elements/in_temp_x_en
# Enable buffer
echo 1 > /sys/bus/iio/devices/iio:device3/buffer0/enable
# Try to stream
iio_readdev -b 256 iio:device3
The driver logs show that st_sths34pf80_preenable() runs, ODR is set, and st_sths34pf80_manage_interrupt_cfg() is called.
However, iio_readdev times out with Unable to refill buffer: Connection timed out.
It looks like no samples are ever pushed into the buffer.
"Enter st_sths34pf80_preenable
Enter st_sths34pf80_sensor_set_enable
odr_value: 4 uodr_value: 0
Enter st_sths34pf80_manage_interrupt_cfg
...
Unable to refill buffer: Connection timed out"
From reviewing st_sths34pf80_core.c, the continuous mode flow is:
preenable() → sensor_set_enable() → manage_interrupt_cfg() → IRQ → irq_thread() → iio_push_to_buffers_with_timestamp().
Currently, it seems that st_sths34pf80_manage_interrupt_cfg() does not program CTRL3.IEN correctly for data-ready interrupts when buffer streaming is enabled.
As a result, no valid data-ready interrupts are generated, so irq_thread never pushes samples to the buffer.
Could you please clarify about this issue? Is there any steps i am missing? Is there any driver edit required?
Thanks advance for your support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.