2007-04-06 4:30 AM
UART - printf on Hyperterminal - STR750 EVAL
2007-04-05 11:11 PM
Hi,
I'm currently trying to display some messages (necessary to debug a more complex application) on the HyperTerminal of Windows, using an UART. I'm working with a STR750-EVAL and the Raisonance IDE (with RLINK). The AN : UM0218 gives a useful example of what i'm trying to do (readme, headers, sources...). (/examples/uart/example 6) My problem is that this example doesn't work. I get nothing on the Hyperterminal when I call the printf function, although I get something when I use the function Uart_SendData(). The main3.c contains a function fputc who is supposed to retarget the C library printf function to the UART. Is this example supposed to work ? (with Raisonance IDE, Rlink, and the files I have attached). Should I re-implement the fputc function in main3.c ? Should I add something else in the ''.c'' files ? Thank you in advance. ________________ Attachments : UART_printf_STR750.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtIh&d=%2Fa%2F0X0000000aLH%2FM13fjexAeH0BZY6VkJHmDXdoWSXZx2iX6jxLdY9Uh_g&asPdf=false2007-04-05 11:14 PM
Hi,
The printf function will call putchar function in the end. So it is putchar, not fputc, that you need to rewrite. Or you can use the default UART0_putchar. See this example: c:\ride\examples\strx\test Best Regards, Vincent2007-04-05 11:18 PM
You will also find some information on the UART0_putchar in this doc:
(in RIDE) ''help''->''PDF''->''STRX-Tools''->''Getting Started STRX'' look in the section about the library options. (section 2.5.1.1, page 14, in the latest version) Vincent2007-04-06 4:30 AM
Thank you for you answer.
For people who are using this example, use the UART1 although the library is called Uart0... (I lost 2 hours :p)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.