2007-05-09 1:33 AM
2011-05-17 12:43 AM
Hi all,
i have the following problem: I run the timer 0 in Output Compare 1 Mode with the interrupt enabled cause i need an 1ms Clock. Now, when an Interrupt occurs, i toggle an LED and i see on my Scope, that the IRQ-Routine is entered 2 times directley next to each other. I have attached my Source-Code. Thanks for Help :) And i also work not with the complicated Libs from ST, i directly uses the Register !!! Michi2011-05-17 12:43 AM
Sorry, this is the Wrong Forum, i need the str9 forum . . .
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.