2007-05-14 8:55 AM
Programming/debugging with IAR's workbench and FlashLINK
2011-05-17 12:43 AM
Is it possible to use the FlashLINK (parallel port) with IAR'a workbench to do programming and debugging ?
Under ''Debugger'' there is an option for ''Third-Party Driver'', so it seems that is possible to use other devices. Any experience using this option ? Regards, Mark.2011-05-17 12:43 AM
I find the Flashlink circuit, along with the Jtag Programmer an excellent tool for programming and for erasing the STR91x ARM processors when the core cannot be stopped using the JLink.
So I think that for debugging, the Flashlink circuit should be a great aid. Does any one have had an experience doing so ? How about a comment from ST side ? MarkWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.