2011-03-25 8:17 PM
Just received my STM8L-Discovery, installed STVD 4.2.1 and Raisonance compiler. Whenever I hit F7, STVD shows this non-descriptive message ''The parameter is incorrect''. After that, the only way to exit the application is to kill it in the Task Manager. I tried it on Win XP and Win 7 (32-bit) with same results.
Does anyone experienced a similar problem? Thanks for help!2011-05-23 11:00 AM
When do you expect the fix to be available?
Thanks, Harry2011-05-24 1:17 AM
2011-05-30 1:19 AM
2011-05-30 2:08 PM
Thanks!
i've this problem and solved with your patch.
2011-07-25 4:33 AM
I've installed V4.2.1 and Patch 2 but still struggling with this problem of ''The parameter is incorrect'' on an ST8 application using the Assembler / Linker toolchain.
I've tried to run the ST7 example 'realtime' supplied and this will not work either. The system loads the mapping.asm and main.asm automatically and when a build is attempted the system reports ST Visual Develop The executable could not be found You can fix it by editing your toolset settings etc. etc. It hangs up while attempting to assemble mapping.asm and reports Error creating process for executable asm The parameter is incorrect Failed to create process. All files ie assembler, linker etc are located in a single project file and this is the path shown in project settings. Any idea what's going on and how I can work round it?2011-08-05 12:59 PM
I've installed V4.2.1 and Patch 2 but still struggling with this problem of ''The parameter is incorrect'' on an ST8 application using the Assembler / Linker toolchain.
I've tried to run the ST7 example 'realtime' supplied and this will not work either. The system loads the mapping.asm and main.asm automatically and when a build is attempted the system reports ST Visual Develop The executable could not be found You can fix it by editing your toolset settings etc. etc. It hangs up while attempting to assemble mapping.asm and reports Error creating process for executable asm The parameter is incorrect Failed to create process. All files ie assembler, linker etc are located in a single project file and this is the path shown in project settings. Any idea what's going on and how I can work round it?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.