2008-01-14 5:00 AM
2007-12-27 12:49 AM
Hello,
I'm encountering problems with I2C Slave operation. Can anyone tell me what the problem is? What am I missing? Any help is appreciated. IHere is my code: I'm also attaching the whole code. // I2C Configuration void I2C_Configuration(void) { I2C_InitTypeDef I2C_InitStructure; /* I2C configuration */ I2C_InitStructure.I2C_GeneralCall = I2C_GeneralCall_Disable; I2C_InitStructure.I2C_Ack = I2C_Ack_Enable; I2C_InitStructure.I2C_CLKSpeed = 100000; I2C_InitStructure.I2C_OwnAddress = 0x02; /* I2C Peripheral Enable */ I2C_Cmd (ENABLE); I2C_ITConfig(ENABLE); // yeni /* Apply I2C configuration after enabling it */ I2C_Init(&I2C_InitStructure); } // EIC Configuration void EIC_Configuration(void) { EIC_IRQInitTypeDef EIC_IRQInitStructure; /* Configure and enable I2C_IRQChannel */ EIC_IRQInitStructure.EIC_IRQChannel = I2C_IRQChannel; EIC_IRQInitStructure.EIC_IRQChannelPriority = 1; EIC_IRQInitStructure.EIC_IRQChannelCmd= ENABLE; EIC_IRQInit(&EIC_IRQInitStructure); /* Configure and enable RTC_IRQChannel */ EIC_IRQInitStructure.EIC_IRQChannel = RTC_IRQChannel; EIC_IRQInitStructure.EIC_IRQChannelPriority = 2; EIC_IRQInitStructure.EIC_IRQChannelCmd= ENABLE; EIC_IRQInit(&EIC_IRQInitStructure); /* ADC IRQ Channel configuration */ EIC_IRQInitStructure.EIC_IRQChannel = ADC_IRQChannel; EIC_IRQInitStructure.EIC_IRQChannelPriority = 3; EIC_IRQInitStructure.EIC_IRQChannelCmd = ENABLE; EIC_IRQInit(&EIC_IRQInitStructure); /* Enable the interrupt controller */ EIC_IRQCmd(ENABLE); } // GPIO Configuration void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; /* SCL and SDA I2C pins configuration */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 ; GPIO_Init(GPIO0, &GPIO_InitStructure); //... } // MRCC Configuration void MRCC_Configuration(void) { /* MRCC system reset(for debug purpose) */ MRCC_DeInit(); /* Wait for OSC4M start-up */ OSC4MStartUpStatus = MRCC_WaitForOSC4MStartUp(); if(OSC4MStartUpStatus == SUCCESS) { /* Set HCLK to 30MHz */ MRCC_HCLKConfig(MRCC_CKSYS_Div2); /* Set CKTIM to 30MHz */ MRCC_CKTIMConfig(MRCC_HCLK_Div1); /* Set PCLK to 30MHz */ MRCC_PCLKConfig(MRCC_CKTIM_Div1); /* Set CK_SYS to 60 MHz */ MRCC_CKSYSConfig(MRCC_CKSYS_OSC4MPLL, MRCC_PLL_Mul_15); } /* GPIO pins optimized for 3V3 operation */ MRCC_IOVoltageRangeConfig(MRCC_IOVoltageRange_3V3); /* Enable GPIO and UART0 clock */ MRCC_PeripheralClockConfig(MRCC_Peripheral_I2C | MRCC_Peripheral_ADC | MRCC_Peripheral_GPIO | MRCC_Peripheral_UART0, ENABLE); // Here is the interrupt ruotine: void I2C_IRQHandler(void) { switch (I2C_GetLastEvent()) { case I2C_EVENT_SLAVE_ADDRESS_MATCHED: // EV1 Rx_Idx = Tx_Idx = 0; break; case I2C_EVENT_SLAVE_BYTE_RECEIVED: // EV2 I2C0_Buffer_Rx[Rx_Idx++] = I2C_ReceiveData(); break; case I2C_EVENT_SLAVE_BYTE_TRANSMITTED: // EV3 I2C_SendData(I2C0_Buffer_Tx[Tx_Idx++]); break; case I2C_EVENT_SLAVE_ACK_FAILURE: // EV3-1 I2C_SendData(0xFF); break; case I2C_EVENT_SLAVE_STOP_DETECTED: // EV4 Rx_Idx = Tx_Idx = 0; break; default: break; } } [ This message was edited by: ucoskun on 02-01-2008 19:56 ]2008-01-14 5:00 AM
It seems to me the problem has nothing to do with the software,interrupt configuration is correct. Perhaps a hardware issue.
Chris.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.