2026-03-12 3:39 AM - edited 2026-03-12 5:57 AM
I am testing the Timer and PWM with different combinations to understand it better on NucleoF446RE board. I have configured as below
Timer1 as Master with trigger output as update event, PWM channel1 output on PA8 (interrupt).
Timer2 as slave in trigger mode and output PWM Channel1 on PA5 same as LED based on interrupt.
Problem is Timer2 Channel1 output does not toggle on PA5 but if i place break point in tiimer2 interrupt is triggered.
void TIM2_IRQHandler(void)
{
/* USER CODE BEGIN TIM2_IRQn 0 */
/* USER CODE END TIM2_IRQn 0 */
HAL_TIM_IRQHandler(&htim2);
/* USER CODE BEGIN TIM2_IRQn 1 */
/* USER CODE END TIM2_IRQn 1 */
}Please guide to solve the issue.
Solved! Go to Solution.
2026-03-12 6:37 AM
> sConfigOC.Pulse = 0;
This produces a DC signal, not a PWM.
2026-03-12 5:01 AM - edited 2026-03-12 5:01 AM
Read out and check/post content of TIM and relevant GPIO registers.
JW
PS. Don't @-invoke users to attract attention. It's inappropriate.
2026-03-12 6:37 AM
> sConfigOC.Pulse = 0;
This produces a DC signal, not a PWM.
2026-03-12 7:28 AM
Yes i have to verifying the register values, it may give some hint of solving the problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.