2008-01-14 5:30 AM
ADC activation with STR750 - I need some help
2007-12-23 3:10 AM
I'm trying to activate the ADC in STR750 without success.
I'm running in a loop waiting for a FLAG to be set for ever Attach below my code Can any one help? ADC setup code: void ADC_setCFG(USHORT ConversionMode, LONG FirstChannel, LONG ChannelNumber) { /* 1: ADC_setCFG() */ ADC_InitTypeDef ADC_InitStructure; ADC_StructInit(&ADC_InitStructure); /* ADC configuration */ ADC_InitStructure.ADC_ConversionMode = ConversionMode; ADC_InitStructure.ADC_ExtTrigger = ADC_ExtTrigger_Disable; ADC_InitStructure.ADC_AutoClockOff = ADC_AutoClockOff_Disable; ADC_InitStructure.ADC_SamplingPrescaler = 32; ADC_InitStructure.ADC_ConversionPrescaler = 32; ADC_InitStructure.ADC_FirstChannel = FirstChannel; ADC_InitStructure.ADC_ChannelNumber = ChannelNumber; ADC_Init(&ADC_InitStructure); } /* 1: ADC_setCFG() */ void ADC_InitHW(void) { /* 1: ADC_InitHW(void) */ EIC_IRQInitTypeDef EIC_IRQInitStructure; FlagStatus CalibrationDone; ADC_DeInit(); MRCC_PeripheralSWResetConfig(MRCC_Peripheral_ADC,ENABLE); ADC_InitInputs(); /* by default set ADC configuration for SCAN mode, starting with inputs 0, and scan all 16 inputs (15 = 16 - 1 , see manual) */ ADC_setCFG(ADC_ConversionMode_Scan, ADC_CHANNEL0, 15); /* Configure the IEC for the ADC interrupts. */ EIC_IRQInitStructure.EIC_IRQChannelCmd = ENABLE; EIC_IRQInitStructure.EIC_IRQChannel = ADC_IRQChannel; EIC_IRQInitStructure.EIC_IRQChannelPriority = 1; EIC_IRQInit(&EIC_IRQInitStructure); ADC_ITConfig(ADC_IT_ALL, ENABLE); /* Enable ADC */ ADC_Cmd(ENABLE); /* Start calibration */ ADC_StartCalibration(ADC_CalibAverage_Enable); CalibrationDone = SET; while (CalibrationDone != RESET) { CalibrationDone = ADC_GetCalibrationStatus(); } } /* 1: ADC_InitHW(void) */ void ADC_Start(void) { ADC_ConversionCmd (ADC_Conversion_Start); } This is the activation code: ADC_Start(); while (1) { adc_flag = ADC_GetFlagStatus(ADC_FLAG_EOC); if (adc_flag == SET) { ADC_ClearFlag(ADC_FLAG_EOC); for (i = 0; i < 16 ; i++) { adc_value = ADC_GetConversionValue(i); } } }2008-01-14 5:30 AM
Are the ADC Channel pin configured? and the GPIO clock enabled?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.