2022-05-07 9:36 AM
Hi there, I'm trying to interface with two different slave devices using the two SPI modules on the STML432kc with Mbed OS. Individually they work fine but as soon as i have both defined in the same program i run into hard faults.
I'm aware of the pin conflict between PA_5, PA_6 , PB_6 and PB_7, however I'm not using PB_6 or 7 and even with SB16 and 18 disconnected im still seeing the same faults.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.