Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

pointer or stack problem?

Posted on September 23, 2014 at 17:41I'm not even sure what to ask so I'll explain the problem as best I can. I did search everywhere for an answer. Anyway, I have an embedded project with a STM8S208C8 micro. I developed the project in C using ST Vi...

crc ccitt 16 bit for stm8s207

Posted on September 19, 2014 at 09:57hello please may i ask if there is a program availabe in assembly language for calculating the crc ccitt  with x16+x12+c5+1 many thanks marc debruyne #crc

Booting Linux or U-Boot via USB boot on SPEAr320

Posted on April 26, 2013 at 09:15Hello Is it  possible to boot Linux Kernel via the  USB boot mechanism in the SPAEr320 CPU? If yes, what tools are available to generate an image for a bootable USB stick? I hope to get at least a link to an approbri...

hj by Associate III
  • 2099 Views
  • 2 replies
  • 0 kudos

IAR OUTPUT FILE

Posted on August 28, 2014 at 11:44Hi Iam new to STM8S,Help me 1) STM8S value line discovery board Connected to the PC 2) EW STM8S Installed 3) compile the sample code -The out put of compile code is not in Hex file.    it is on .outfile. HOW TO CH...

baskaran by Associate
  • 938 Views
  • 0 replies
  • 0 kudos

ADC1 with with COMP1?

Posted on August 21, 2014 at 21:18Hello,I am working on an application which requires the use of the ADC1 peripheral as well as the COMP1 & COMP2 peripherals. There does not appear to be anything in the datasheet against this, but there is a note in...

gtrotter by Associate
  • 781 Views
  • 0 replies
  • 0 kudos

Swim protocol

Posted on August 08, 2014 at 13:36I'm trying to program an stm8s105 using  icp method through the swim interface and using an STM32F4 discovery board as host and a firmware written by me. I can enable the swim interface of the stm8s and i can read a...

angelo_pa by Associate II
  • 1942 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.