2019-11-12 2:27 AM
#include "stm8s.h"
//My delay for testing. Calibrated for milli seconds.
void delay2(uint16_t ms)
{
volatile uint16_t a = 100;
while(ms--) {
a = 1800;
while(a--);
}
}
void main(void)
{
//CLK_DeInit();
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
/* Clock divider to HSI/1 */
//CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV128);
//CLK_ClockSwitchConfig(CLK_SWITCHMODE_MANUAL, CLK_SOURCE_LSI, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
/* Initialize LEDs in Output Push-Pull Mode */
GPIO_Init(LED_PORT, (LED_PIN), GPIO_MODE_OUT_PP_LOW_FAST);
/* Initialize PB0 (BUTTON) in Input Pullup Mode with Interrupt */
GPIO_Init(BUTTON_PORT, BUTTON_PIN, GPIO_MODE_IN_PU_IT);
/* Initialize the Interrupt sensitivity */
EXTI_DeInit();
EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOC, EXTI_SENSITIVITY_FALL_ONLY);
EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_FALL_ONLY);
enableInterrupts(); //GPIO ISR is not populated because I am using it to just wakeup CPU.
int i;
for( i = 0; i < 10; i++) { //RESET DETECTION CODE
GPIO_WriteLow(LED_PORT,LED_PIN);
delay2(100);
GPIO_WriteHigh(LED_PORT,LED_PIN);
delay2(100);
}
//APPLICATION TEST CODE TO FIND RESET BUG. It is toggling the LED on button click, but occasionally chip is getting reset.
while(1) { //CHIP IS RESETTING OCCASIONALLY WHILE I am continuously triggering the button !!!! I don't know why...
halt(); //Push button press will wake it up.
GPIO_WriteLow(LED_PORT,LED_PIN); //Ignoring debounce while testing...
halt(); //Push button press will wake it up.
GPIO_WriteHigh(LED_PORT,LED_PIN); //Ignoring debounce while testing...
}
}
I haven't changed any option bytes and what ever is there by default is still there.
Also I haven't configured any watchdog and I am not finding any watchdog reset issue because if I am not pressing the button, the LED state is not changed that means the chip is not resetting. But while I am pressing the button, one out of 10 time or one out of 20 times it resets the chip. I haven't configured anything before using halt() feature, I just measured the current at default halt mode and I am okay with it, so I just continued using it. But now I am facing occasional chip reset or very rare chip hanging.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.