Operating temperature range of this IC "STTH112A-TR"
Can i know the minimum Operating temperature of this IC "STTH112A-TR"will it support negative temperature "-40"
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Can i know the minimum Operating temperature of this IC "STTH112A-TR"will it support negative temperature "-40"
Hi. I'm writing assembler code for the STM8S001j3. The data sheet recommends setting ports E5 & F4 to lo for power useage & EMC reasons. However the .asm & .inc files called up do not define ports E or F. The same goes for the peripheral enable regi...
Is there a general statement on PFAS for ST Micro products? If not, can you advise if the part below contain PFAS?L78L15ACUTR
Hello,I am doing simulations with the LM2903 comparator to evaluate if it is suitable for my application. The datasheet indicates that this device can operate at temperatures up to 125 ºC. However, when I increase the temperature, at 90 ºC the output...
Hello, I am using the LDK320M-R, Linear Voltage Regulator IC with Positive Adjustable Output, in one of my current projects. The data sheet states that the ADJ pin voltage range is from - 0.3 to 2V, but does not show how this voltage range configures...
Hello everyone, for testing the Eval Board EV-L99LDLH32GEN, what USB-CAN FD adapter do I have to use between our laptop with the "STSW-EVLDLH32GEN" installed software and the Cannon 9M/Male CAN FD connector of the Eval board?Are these options possibl...
Need to know:What is the material attached with the die to the lead frame for this microcircuits part STM811TW16F? gold wire bond or coper wire bond or other?
we are noticing some failure SPV1040 in our implementation on a board for energy harvesting from solar panel. The breakdown is only for SPV1040. Short between GND and Vout. Attached schematic for your reference.we have taken the reference design of S...
Hi,I am trying to figure out which TOL Sensor to use for a robot application.Usecase: Distance measurement on coated shiny metal surfaces while moving over them, to detect an edge. Detection Range 10-50mm (if it detects further that would be fine, bu...
Hi Team,I am testing in LSM6DSL and I have a problem with accelerometer data reading.I am getting 12.73 read/sec while setting 80ms as a timeout in application and getting accurate accelerometer values. If I decrease the timeout less than 80ms, it wi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.