2003-04-11 10:32 AM
2011-05-17 2:33 AM
On page 5 of version 1.7 of the ST9F150/F250 Errata Sheet (Sept 2002),
there is a work-around to correct software reset. It states to set the XT_DIV16 bit which is bit 1 but bit 1 is LOCK. XT_DIV16 is bit 4. Could you let me know which to set? XT_DIV16 or LOCK? Same question for CKAF_SEL which is bit 32011-05-17 2:33 AM
You are correct regarding your first comment (that's a typo). CKAF_SEL is however located in bit 2 and not bit 3.
You should have read : Before generating a software reset, select CLOCK2 as Internal Clock. To do this: – Reset the CSU_CKSEL bit (Bit 0 of CLK_FLAG, R242 page 55), – Set the XT_DIV16 bit (Bit 3 of CLK_FLAG, R242 page 55), – Reset the CKAF_SEL bit (Bit 2 of CLKCTL, R240, page 55). JojoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.