2004-01-27 7:50 PM
2004-01-27 3:55 PM
Hi,
I define the PA0 as ei0 int pin. The sensitivity is ''Falling edge only'', I am sure that the EICR = #$06 and EISR = #$0c , they were set just after power on reset, and no modification is done after then. Now the question is: An interrupt is generated by both falling edge and low level . I have observed there is no falling edge occured during the low level period. Thanks, J.V.2004-01-27 5:57 PM
It is not the normal behavior. Please make sure the interrupt pin is configured in the input pull up mode. Also check it by modify/rewrite the sensitivity bits with in the interrupt routines. If the problem is due to pending interrupts then it should be removed.
[ This message was edited by: Jatin on 28-01-2004 07:28 ][ This message was edited by: Jatin on 28-01-2004 07:29 ]2004-01-27 7:50 PM
Hi Jatin,
As you said, it is caused by pending interrupt. Thank very much! J.V.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.