2003-10-22 7:06 PM
ST7FLITE29, PWM out stays HIGH in HALT - mode
2003-10-13 9:10 PM
In order to save energy in the battery during 'stand-by' we use the HALT mode of the ST7FLITE29.
It seems to work correctly and the current consumption is really very much reduced. But very often, the PWM2 output goes HIGH after the HALT instruction. That must be avoided in the application. The stand-by routine in C is: ClearBit(PWMCR,TWO) // Disable PWM1 .. relay_off(); // Turn all outputs OFF .. ClearBit(PWMCR,FOUR); // Disable PWM2 ClearBit(PADR,FOUR); // Reset PA4 (=PWM2) (not necessary) WDGCR|=0x7F; // watchdog set ClearBit(LTCSR1,TB1IE); // active HALT disabled ClearBit(ATCSR,OVFIE); // '' ClearBit(PADR,FOUR); // to be sure, that the output is LOW in HALT (should not be necessary) Halt; // HALT instruction Several times, the PWM2 (=PA4) output is set LOW. Does anybody have any idea, why it still stays HIGH in HALT mode? We do have the problem only with the PWM2 and not with PWM1, although they are connected electrically in the same way. Thank you all for help!2003-10-22 7:06 PM
If we add a delay of one second between stopping the PWM and the HALT command it works correctly. The PWM output stays LOW during HALT.
But why? Anybody an idea? Thank you for any hints!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.