2005-10-23 8:46 PM
2005-03-04 4:33 AM
Hi Shinn,
Please try this software. Best regards Prog 8-) ________________ Attachments : rtc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtKr&d=%2Fa%2F0X0000000aLg%2FlPnRAnKDzAetEregJdTLcKSY5t2DgN120jvMJfHjjUo&asPdf=false2005-03-06 3:21 PM
2005-10-06 11:08 PM
I am doing the same kind of test but with the alarm interrupt.
When I enter LPWFI mode I cannot catch the RTC IT. I don't test with the Second Interrupt but with the alarm It doesn't work. Is there a solution? I test with the XTI line 15 interruption and it works! But why ? Here is some explaination If I simulated LPWFI that way : #if 1 int i=0; while(i AsystTrace(''> %d %d\n'', RTC->CNTL, _n_step); // _n_step the alarm timer i++; for (int j=0;j } #else PCU_WFIEnter(WFI_EXTERNAL,ENABLE,ENABLE); #endif If I use: RCCU_RCLKSourceConfig(RCCU_RTC_CLOCK); Not IT catch and I see : > 1016 3328 > 1016 3328 > 1016 3328 > 1016 3328 > 1016 3328 with RCCU_RCLKSourceConfig(RCCU_CLOCK2_16); Interrupt is caught and I see > 1010 3328 > 1261 3328 > 1511 3328 > 1759 3328 > 2012 3328 > 2263 3328 > 2511 3328 > 2764 3328 > 3017 3328 > 3265 3328 Haaaaa! > 3346 3328 > 3362 3328 > 3382 3328 > 3399 3328 > 3419 3328 > 3440 3328 > 3460 3328 > 3480 3328 > 3501 3328 > 3517 3328 And the RTC_Handler __arm void RTC_IRQHandler(void) { ... if ( RTC_FlagStatus ( RTC_AIR ) == SET ) { RCCU_RCLKSourceConfig(RCCU_CLOCK2); // To enable the bus between RTC and APB RTC *4 < CORE AsystTrace(''Haaaaa!\n''); RTC_FlagClear ( RTC_AIR ); RTC_FlagClear ( RTC_GIR ); } ... }2005-10-23 8:46 PM
Hello,
I noticed that : To be caught, the RTC component must be scheduled by RCCU_PCLKConfig(RCCU_DEFAULT);. If not, the RTC Alarm IT cannot be caught surely. is that true ? LudoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.