2023-10-03 11:24 PM
We need a microcontroller 8BIT 32KB FLASH 64QFP. we used MC68HC908AB32CFU that is NXP part now we want to go in STM microcontroller . Please suggest if which part is compatible with it.
Thanks and Regards Pooja Katariya
2023-10-04 4:51 AM
I recommend STM8S207R6 (32KB) or STM8S207R8 (64KB), see: STM8S207/208.
2023-10-04 5:20 AM
Not likely to be anything close to pin or code compatible.
Why 8-bit? Consider 32-bit STM32 Cortex-M0(+) type parts with more and current tool availability. Free Keil, free GNU based
Consider STM32C0 and STM32G0 families. Write in C, and port over application
What OTHER requirements do you need, size of FLASH perhaps doesn't directly correlate? Might indicate code complexity, 32-bit might do some operations more efficiently, good use of subroutines, and optimization can also help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.