Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8 internal temperature sensor

Posted on September 06, 2016 at 10:20I am working on a project, which is based on STM8 MCU. I am using ADC to read the ambient temperature. Sometimes I am getting temperature ADC readings which are greater than the usual ones. Most of the time the s...

jakub23 by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

ADC interrupt in cosmic

Posted on November 16, 2016 at 12:55Dear all I tried to read  ADC1 channels in stm8 in cosmic compiler, but still I could not. as far as the main program start to config the ADC1 initialization nothing happen. I do not know what the problem is with ...

Resolved! STM8 and STVP: how to flash .HEX file

Posted on November 21, 2016 at 13:34Hi everyone. I have an .HEX file that I would like to program in a STM8AF62A8 MCU. I load the .HEX into STVP and it seems to be flashing the memory correctly because I can see some of the application's startup ou...

jorge23 by Associate
  • 2286 Views
  • 1 replies
  • 0 kudos

HVLED001 eDesignSuite vs Datasheet

Posted on November 14, 2016 at 19:03Hi There,After using the eDesignSuite to design a 25V (CV / HPF / PSR) using the HVLED001, we found some discrepancies between the eDesignSuite proposed circuit and the HVLED001 typical HPF / PSR / CV circuit on p...

ppereira by Associate II
  • 3973 Views
  • 7 replies
  • 0 kudos

LED5000

Posted on June 09, 2015 at 10:44My customer wants to use A/LED5000 to design Automotive lightingVin=10~30V, Vout=30V/1.4~1.5A, LED=CREE XLamp XP-G2 series(Vf=3V, If?1.5A)It's possible to use Floating Boost circuit to design LED5000 on this project o...

HVLED815PF on Power Supply eDesignSuite

Posted on November 16, 2016 at 11:30Hi There,It would be great to be able to choose HVLED815PF on eDesignSuite, when selecting:Power Conversion -> Power Supply -> AC/DC -> Isolated -> QR Flyback (with HPF), instead of only as LED Driver. The purpose...

ppereira by Associate II
  • 1514 Views
  • 2 replies
  • 0 kudos

SPEAR 1340 PCIE controller FC credits

Posted on November 15, 2016 at 13:05Hi, Is there anyway to know the currently consumed FC credeits versus the available cerdits in the Spear PCIE controller [RC mode]. We are seeing an issue where the system gets external data abort after running fo...

st10f273m can bootstrap

Posted on November 13, 2016 at 23:02does anyone can share bootstrap loader and monitor to proceed st10f273m CAN bootstrap? i can successfully enter to BSL over CAN, sending frame 0 with DLC 0 and after 128 frames with id 5 and first byte of my code....

lingo by Associate II
  • 1244 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.