2026-04-15 11:17 PM
Hi All,
I’m working on a project using an 8-bit microcontroller connected to an ST25DVXXKC NFC chip over I²C. The standard NFC features are working correctly, and the code is already in production.
Now I’m trying to implement Fast Transfer Mode (FTM) for OTA updates and bidirectional data transfer between the microcontroller and the NFC reader.
I’m currently using ST’s ST25FTM library and the ST25DV64KC-DISCO Kit v2.2.1 package, but I’m confused by the available examples and documentation, which seem limited and unclear regarding how to properly port and use the library.
In the v2.2.1 package, there is a Demonstrations folder containing two projects:
From my understanding:
I have tried porting ST25DVDemo_FwUpgd to my 8-bit MCU platform. Some features work (e.g., enabling Fast Transfer Mode and reading device version), but the firmware update process is not working correctly—specifically, the password command for firmware update is not being recognized.
I also attempted to port ftm_demo.c from the ST25DVDemo project, but it does not function properly on my setup.
At this point, I’m unclear on:
I’ve attached screenshots for reference.
Solved! Go to Solution.
2026-04-20 5:16 AM
Hello SamP,
You only need to focus on the ST25DVDemo project, the other is only used to generate a binary file for the firmware upgrade demo. The ST25DVDemo_FwUpgd project is not updated and it is maintained as is (source files are older version), it shows only one or two features (generated binary is approximately 32KB, compared to 375KB for the main firmware ) to simulate the upgrade of a new firmware (but after a reset, the system reverts to the main firmware).
Hope this can help you.
Kind Regards.
2026-04-20 5:16 AM
Hello SamP,
You only need to focus on the ST25DVDemo project, the other is only used to generate a binary file for the firmware upgrade demo. The ST25DVDemo_FwUpgd project is not updated and it is maintained as is (source files are older version), it shows only one or two features (generated binary is approximately 32KB, compared to 375KB for the main firmware ) to simulate the upgrade of a new firmware (but after a reset, the system reverts to the main firmware).
Hope this can help you.
Kind Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.