2003-03-31 11:10 AM
PSD 3200 XRAM space in von neumann mode
2011-05-17 2:53 AM
Hi guys,
is there a way to set the 8 KB internal XRAM space in Von Neumann mode ? I would use it with keil's MON51 to test small programs (and not)2011-05-17 2:53 AM
Yes, the uPSD's SRAM can be setup using the Von Neumann architecture. When bit 0 of the VM register is set, _PSEN is used to access the SRAM as Program space. When this bit is cleared, _RD , is used to access the SRAM as DATA space. Please see page 117 of the uPSD323x data sheet for a graphical explaination.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.