2003-04-04 1:37 AM
2011-05-17 2:53 AM
Is there a solution to erase one byte in the flash in order to reprogram it with a new value? I try to use it as an eeprom and i don't want to erase all the block to reprogram it
Thanks, Sebastien2011-05-17 2:53 AM
You can't erase a byte in the flash, because a block can be erase in the flash.
There is a idea to erase a byte: 1. you copy the block to RAM 2. erase the block 3. change the byte which you want to erase. 4. write them to the block.2011-05-17 2:53 AM
Yes, you can update one byte at a time using the attached EEPROM emulation code.
2011-05-17 2:53 AM
Thank you , iy works...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.