2003-06-09 1:50 AM
2003-06-02 4:54 AM
Hye,
I'm trying to program in ISP mode an ST72C215G2 via an ST7MDT1-DVP2 KIT. My OS is Windows XP Home edition... And just before achieving the programmation, it stopped on the error listed above. Why ?! I tried on another PC under Windows 98...It works well !!! Please, what can I do ?2003-06-05 3:20 AM
Hello,
What version of STVD7 are you using? I would suggest STVD7 2.5.2. During the installation process, you must have been asked for installation of parallel port driver. Is this driver installed?2003-06-05 4:59 AM
Hello,
I'm using the STVD7 V2.5.2, but the problem is with the STVP Version 1.8. The parallel port driver is installed ?!2003-06-09 1:50 AM
Some suggestions :
1) The parallel port driver for the STVP7 should have been installed during STVP7. Please re-install and check. 2) Is the hardware of your kit updated?(Refer AN1363)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.