2007-09-02 9:21 PM
Problem with DMA and VIC. Interruption launched only one time. Again...
2011-05-17 12:46 AM
Hello,
I have posted a message about a problem I have with the timer and interruption. Because i can have one interruption, and no more. I work too with DMA, and it must set an interrupt when it has finish a transfer. And for the first transfer i have an interruption, but not for the others (I'm sure all the transfer are done). I don't understand. I look a project (AN2442) which work with dma and interruption, and i do the same configuration for DMA and VIC. So, i really don't understand why i have this problem. Here the initialization code :Code:
// For VIC VIC_DeInit(); // Reset values VIC_Config(DMA_ITLine, VIC_IRQ, 0); // Configure for generate IRQ VIC_ITCmd(DMA_ITLine, ENABLE); // Active interrupt from DMA // For DMA LLI2_InitStruct.LLI_SrcAdd = (u32)((&SSP1->DR)); // Source address is FIFO on SSP1 LLI2_InitStruct.LLI_DesAdd = (u32)(&BufferIn2[0]); // Destination address is the second input buffer LLI2_InitStruct.LLI_Pointer = 0; LLI2_InitStruct.LLI_CCR = 0x88240100; // Control Word : transfer of 256 bits SSP DMA_DeInit(); // Reset values DMA_StructInit(&DMA_InitStruct); // Initialize structure DMA_InitStruct.DMA_Channel_LLstItm = (u32)(&(LLI2_InitStruct.LLI_SrcAdd)); // Branch on second LLI DMA_InitStruct.DMA_Channel_SrcAdd=(u32)((&SSP1->DR)); // Source address is FIFO on SSP1 DMA_InitStruct.DMA_Channel_DesAdd=(u32)(&BufferIn1[0]); // Destination address is the first input buffer DMA_InitStruct.DMA_Channel_SrcWidth = DMA_SrcWidth_HalfWord;// Source width is 16 bits DMA_InitStruct.DMA_Channel_DesWidth = DMA_DesWidth_HalfWord;// Destination width is 16 bits DMA_InitStruct.DMA_Channel_DesBstSize = DMA_DesBst_1Data ; // Source burst transfer request is 1 data DMA_InitStruct.DMA_Channel_SrcBstSize = DMA_SrcBst_1Data ; // Destination burst transfer request is 1 data DMA_InitStruct.DMA_Channel_Src = DMA_SRC_SSP1_RX; // DMA is programmed for SSP0 in transmitter DMA_InitStruct.DMA_Channel_FlowCntrl = DMA_FlowCntrl2_DMA; // The flow controller is the DMA for peripheral to memory transfer (DMA do only ''DMA_Channel_TrsfSize'' transfers, after it load LLI) DMA_InitStruct.DMA_Channel_TrsfSize = 256; // Transfer size of 256 bytes DMA_ChannelDESIncConfig(DMA_Channel0, ENABLE); // Increment the destination not the source DMA_ITConfig(DMA_Channel0, ENABLE); // Active TCIE (Terminal Count Interrupt Enable) DMA_ITMaskConfig(DMA_Channel0, DMA_ITMask_ITC, ENABLE); // Active ITC (Terminal Count Interrupt Mask) DMA_Init(DMA_Channel0,&DMA_InitStruct); // Initialize DMA Channel 0 DMA_ChannelCmd (DMA_Channel0,ENABLE); // Enable DMA Channel 0 DMA_Cmd(ENABLE); // Enable DMA -> Launch Transmission here the interrupt function :Code:
void DMA_IRQHandler(void) { NewFrame++; DMA_ClearIT(Channel0, DMA_TCC); } Help, please, there is something very strange with these interruptions.2011-05-17 12:46 AM
You have to reconfigure the dma in order to get another irq.
2011-05-17 12:46 AM
Code:
LLI2_InitStruct.LLI_CCR = 0x88240100; No ?2011-05-17 12:46 AM
Yes the VIC is enable.
For DMA, when it has finished his first transfer, it load LLI, so it is reinitialized. The second transfer is well done, so the DMA is well reinitialized, but the interruption is not handled. I have a similar problem with timer, so i think there is a problem with the vic, not the DMA. But I don't see what can it be.2011-05-17 12:46 AM
hi,
did you enable the vic peripheral? SCU_AHBPeriphClockConfig(__VIC,ENABLE); /*give the clock to VIC.*/ In any case when I wrote ''reconfigure the DMA'' i mean that the dma registers have to be reinitialized after the dma transfer is done eg. DMA_Channel0->SRC = YOUR_SRC_ADRESS; DMA_Channel0->DES = (u32)Your_first_buffer; /* Set the linked list Items address */ DMA_Channel0->LLI = DMA_Link1[2]; DMA_Channel0->CC = DMA_Link1[3];We’re moving the ST Community to a new platform to give you a better and more reliable community experience.