2009-01-15 2:32 PM
problem configuring STR912 port as external interrupt
2011-05-17 12:57 AM
I got it. It seems that the library version i have does not have all the requisite functions such as VIC_InitDefaultVectors(), so I added few lines as :
VIC0->DVAR = 0xffffffff; VIC1->DVAR = 0xffffffff; I was able to get it running. However, can you please suggest me place for the updated libraries. I am using IAR for compiling. Thanks again for your help.[ This message was edited by: dk_vhd on 13-01-2009 19:58 ]2011-05-17 12:57 AM
I am a newbie am working on a STR912 development board. I want to use external interrupt for IR interface (such as remote). I am using the following configuration in main function :
GPIO_DeInit(GPIO3); GPIO_Struct.GPIO_Pin= GPIO_Pin_2; GPIO_Struct.GPIO_Direction=GPIO_PinInput; GPIO_Struct.GPIO_Type=GPIO_Type_PushPull; // GPIO_Struct.GPIO_Alternate = GPIO_InputAlt1; GPIO_Struct.GPIO_IPConnected = GPIO_IPConnected_Enable; SCU_WakeUpLineConfig(2); GPIO_Init(GPIO3,&GPIO_Struct); I am trying to use EXTIT2() handler function provided in 91x_it.c. However I cannot make it work. How do I setup the code to access this handler ? Can somebody help please... Thanks in Advance2011-05-17 12:57 AM
Hi dk_vhd,
Looking to your peace of code, you are not using the right external interrupt line. In fact, the external interrupt triggered through Pin 3.2 belongs to EXTIT0_ITLine, hence you have to use EXTIT0_IRQHandler() instead. Moreover you are not obliged to configure GPIO3.2 since the Default Input Function of the pin is as external interrupted pin. Please find attached a main program showing to you how to proceed. Kind regards, Eris.2011-05-17 12:57 AM
Hi,
You can download the last STR9 firmware library, directly from ST web site:http://www.st.com/stonline/products/support/micro/files/um0233.zip
Regards, Eris.2011-05-17 12:57 AM
After I have intialized the interrupt, my next step is to start a timer which I have done as follows:
... TIM_InitStructure.TIM_Mode = TIM_OCM_CHANNEL_1; TIM_InitStructure.TIM_OC1_Modes = TIM_TIMING; TIM_InitStructure.TIM_Clock_Source = TIM_CLK_APB; TIM_InitStructure.TIM_Clock_Edge = TIM_CLK_EDGE_FALLING; TIM_InitStructure.TIM_Prescaler = 0x64; TIM_InitStructure.TIM_Pulse_Length_1 = 0x3BB; TIM_Init (TIM0, &TIM_InitStructure); /*Enable TIM1 Output Compare1 Interrupt */ TIM_ITConfig(TIM0, TIM_IT_OC1, ENABLE); However, I still have to stop the code from executing EXT0_IRQHandler() repeatedly. Can I use WIU_ClearITPendingBit(WIU_Line2) funtion to clear the recieved interrupt ? Also, same would be needed for the timer as well. I am not sure if the above method is good way to generate a timer interrupt for waiting for real time (say 100 ms) ? Infact I am using the following routine in the EXTIT0_IRQHandler() function: VIC0->VAR = 0xffffffff; VIC1->VAR = 0xffffffff; However, the interrupt dont seem to be stopping and is entering into IRQ handler function repeatedly. Can you suggest me how to stop this repeated occurence ? Thanks in Advance [ This message was edited by: dk_vhd on 16-01-2009 17:49 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.