2012-05-23 7:11 AM
The linker is not case sensitive unless the -C flag is used on the command line
Does anyone know how to pass this flag from within ST Visual Develop? I can't just add -C as a user flag as STVD already passes -P and to the linker and the raisonance linker only accepts -CP not -P and -C as separate arguments. How do I replace -P with -CP in STVD? For example, can I stop STVD passing -P so I can add the -CP flag?If the linker is not case sensitive then the c source code needs to be written to avoid the linker seeing, for example, BOB and bob as the same symbol. Which is giving me major code reuse problems. #stvd-raisonance-linkerWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.