2012-05-23 4:00 AM
I am using STVD 4.3.1 with ST-LINK and windows 7 32bit.
Most times I try to enter debug mode I get COMM TIMEOUT ERROR. Clicking STOP and trying again just results in the same error over and over again.The only way to clear the error is to unplug the ST_LINK form the USB, restart STVD and power cycle the target ( not sure if this is necessary ).I have seen other posts reporting the same problem but with no solution.I have upgraded my ST-LINK to the latest firmware and upgraded the windows driver but the problem persists. I think it started when I upgraded STVD.Anyone seen this problem / solved it ?2012-06-07 7:29 AM
This is solved
Turned out to be a noise problem when the target was connected to a bed of nails test jig.2012-06-22 12:09 AM
I've been suffering from the same problem. By yesterday, I had been using ST-Link-2, EWSTM8 of IAR, Win XP. From now on, I have Win 7, but it haven't changed anything.
I turned to both IAR & ST support with the problem, but meanwhile I haven't got an answer.I have a few general ideas what could be a reason for the problems, and will try to check them on the next working week.1. There is a problem with debugging channel when any of Low power modes is being used,i.e. if debugger tries to communicate with MCU, while the latter is in Low power mode, apparently, you should get this kind of error. For debugging period I canceled using of Active halt mode and, instead, I have been using a simple loop, simulating 100msec of Halt mode. However, in addition to the Active Halt mode, I use also Wait mode for short periods of 20-30 us, every 100msec. So, I suspect that sometimes ST-LINK fails when tries to communicate in this time. It's a bit difficult to me to replace this code with a simulation loop,but if I manage to do that, I will know for sure that this is not the reason for the problem. Do you use any of Low power modes ?2. I frequently use Live watch with a dozen of variables inside. I'm not sure, but it seems to me as the more variables inside Live watch, the problem happens more frequently. 3. Do you have any serial resistor on SWIM pin ? If so, remove it, to decrease to a smaller value. In the Discover board, ST do not put any serial resistor on the SWIM channel. The problem with resistor is as SWIM is very high speed communication channel and any resistance disturb to it. We have 47Ohm, and next week I will try to remove it and to see if the problem exists.If you have some findings, would you be so kind as to share them here on the forum ?Thanks,E.L.2012-06-22 12:12 AM
Sorry, it seems as I'm blind. You already posted here the solution, but I have not seen that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.