2024-10-19 12:44 PM
Hello,
I continue my journey toward build a STM32 hardware emulator for the famous Apple II Disk II.
I am implementing UF2 firmware management, USB drag & drag update.
the new firmware is not starting, even if I see log of tinyuf2 passing to the app
and I do not understand why
I put the boot loader (tinyuf2) and I changed :
- system_stm32f4xx.c and I add
/*
******************************************************************************
**
** @file : LinkerScript.ld
**
** @author : Auto-generated by STM32CubeIDE
**
** @brief : Linker script for STM32F411CEUx Device from STM32F4 series
** 512Kbytes FLASH
** 128Kbytes RAM
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used
**
** Target : STMicroelectronics STM32
**
** Distribution: The file is distributed as is, without any warranty
** of any kind.
**
******************************************************************************
** @attention
**
** Copyright (c) 2023 STMicroelectronics.
** All rights reserved.
**
** This software is licensed under terms that can be found in the LICENSE file
** in the root directory of this software component.
** If no LICENSE file comes with this software, it is provided AS-IS.
**
******************************************************************************
*/
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
FLASH (rx) : ORIGIN = 0x08010000, LENGTH = 448K
}
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data into "FLASH" Rom type memory */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data into "FLASH" Rom type memory */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : {
. = ALIGN(4);
*(.ARM.extab* .gnu.linkonce.armextab.*)
. = ALIGN(4);
} >FLASH
.ARM : {
. = ALIGN(4);
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
. = ALIGN(4);
} >FLASH
.preinit_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
. = ALIGN(4);
} >FLASH
.init_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
. = ALIGN(4);
} >FLASH
.fini_array :
{
. = ALIGN(4);
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
. = ALIGN(4);
} >FLASH
/* Used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections into "RAM" Ram type memory */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM AT> FLASH
/* Uninitialized data section into "RAM" Ram type memory */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM
/* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM
/* Remove information from the compiler libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}
What can I do to figure out where is the issue ?
thanks
Vincent
Solved! Go to Solution.
2024-10-21 7:13 AM
Hello Jan,
Ok I found this issue, the jump is correctly made, but the app is crashing at
2024-10-20 11:25 PM
I further investigate the issue and I have to admit that I am really stuck and I have tried many things.
the bootloader is working fine and launching an Arduino simple pin C13 blinking app.
I have written a small app that is doing the same but with vscode makefile...
the app is working when upload and starting at 0x08000000U
Now I want it to start with the UF2 bootloader so I defined the
2024-10-20 11:33 PM - edited 2024-10-20 11:34 PM
Don't change the VECT_TAB_OFFSET - it's relative to the app base set in the linker script file, so it should stay at 0.
My recommendation is to remove the VTOR setting from system_... file and set the VTOR in the bootloader just before starting the app, as shown in some recent topics of bootloader problems.
2024-10-21 12:44 AM
Ok,
so commented line in system_stm32f4xx.c
#if defined(USER_VECT_TAB_ADDRESS)
// SCB->VTOR = VECT_TAB_BASE_ADDRESS | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM */
#endif /* USER_VECT_TAB_ADDRESS */
#if defined(USER_VECT_TAB_ADDRESS)
/*!< Uncomment the following line if you need to relocate your vector Table
in Sram else user remap will be done in Flash. */
/* #define VECT_TAB_SRAM */
#if defined(VECT_TAB_SRAM)
#define VECT_TAB_BASE_ADDRESS SRAM_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#else
#define VECT_TAB_BASE_ADDRESS FLASH_BASE /*!< Vector Table base address field.
This value must be a multiple of 0x200. */
#define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.
This value must be a multiple of 0x200. */
#endif /* VECT_TAB_SRAM */
#endif /* USER_VECT_TAB_ADDRESS */
my LD file has
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
BOOT_FLASH (rx) : ORIGIN = 0x8010000, LENGTH = 16K
EEPROM_EMUL(xrw) : ORIGIN = 0x8014000, LENGTH = 16K
FLASH (rx) : ORIGIN = 0x8018000, LENGTH = 512K - 16K - 16K
}
_EEPROM_Emul_Start = ORIGIN(EEPROM_EMUL);
_EEPROM_Emul_Sector = 1;
/* Sections */
SECTIONS
{
/* The startup code into "FLASH" Rom type memory */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >BOOT_FLASH
My boot loader (tinyUF2) jump with
SCB->VTOR = (uint32_t) 0x08010000;
// Set stack pointer
__set_MSP(sp);
__set_PSP(sp);
// Jump to Application Entry
//asm("bx %0" ::"r"(app_entry));
asm("bx %0" ::"r"(0x08010000));
but still the app is not starting...
Vincent
2024-10-21 4:32 AM
I have checked that I have the firmware successfully in the flash at address 0x08010000.
But the firmware app refuse to start.
How can I solve this ?
Thanks
Vincent
2024-10-21 7:05 AM
Using debugger find out where does the program run (where is PC).
JW
2024-10-21 7:13 AM
Hello Jan,
Ok I found this issue, the jump is correctly made, but the app is crashing at
2024-10-21 8:37 AM
inside SystemClock_Config()
call to
if (((RCC_OscInitStruct->PLL.PLLState) == RCC_PLL_OFF) ||
(READ_BIT(pll_config, RCC_PLLCFGR_PLLSRC) != RCC_OscInitStruct->PLL.PLLSource) ||
(READ_BIT(pll_config, RCC_PLLCFGR_PLLM) != (RCC_OscInitStruct->PLL.PLLM) << RCC_PLLCFGR_PLLM_Pos) ||
(READ_BIT(pll_config, RCC_PLLCFGR_PLLN) != (RCC_OscInitStruct->PLL.PLLN) << RCC_PLLCFGR_PLLN_Pos) ||
(READ_BIT(pll_config, RCC_PLLCFGR_PLLP) != (((RCC_OscInitStruct->PLL.PLLP >> 1U) - 1U)) << RCC_PLLCFGR_PLLP_Pos) ||
(READ_BIT(pll_config, RCC_PLLCFGR_PLLQ) != (RCC_OscInitStruct->PLL.PLLQ << RCC_PLLCFGR_PLLQ_Pos)))
#endif /* RCC_PLLCFGR_PLLR */
{
return HAL_ERROR;
}
2024-10-21 9:21 AM
You'd need to inter-stage, where you call the configuration, say enabling HSI, and MCU clocking, and then call a second time to switch back to the PLL with a new setting.
If the loader's already set clocks optimally for the board, no point in tearing down and redoing.
Perhaps test/check the mode and run code accordingly?
2024-10-21 9:24 AM
Also get Error_Handler() and HardFault_Handler() output actionable data rather than dying silently in a while(1) loop, whilst you scratch your head wondering wtf happened.
Pass __FILE__ and __LINE__ to Error_Handler() to determine where of a dozen places it threw the error.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.