2004-08-05 12:00 AM
Need some help in flashing str71xdemo_gp.axf
2004-08-04 8:21 PM
Hi
I am trying to flash the code (str71xdemo_gp.axf) to ST Micro's evaluation board MB393B through ARM realView ICE ( JTAG Emulator). Processor: STR710FZ2T6. I want to use the embeded (internal) flash. During the time of flashing I have maintained the following boot settings: ( RAM MApped at 0h) BOOTEN:1 BOOT0:0 BOOT1:1 I could succesfully flash the code. Swicthing off the supply, I changed my boot configuration settings to USER mode ( Flash mapped at 0h) to run the program. BOOTEN:0 BOOT0:0 BOOT1:0 But I am not finding anything on the LCD Display. I am not in a position to findout whether the program is correctly booting from internal flash. Can anybody help me in giving the correct procedure( step-by-step) of flashing this code, all the necessry H/W settings to be maintained on the board. Also tell me Is this, the only file ( str71xdemo_gp.axf)I have to use for flashing or any other associated files are required along with this. If so please mention the same.2004-08-04 9:34 PM
Hi
I have used this evaluation board for other purposes during my project development.The board is working fine. But during that time i was using the debugging environment. Now I am trying to flash the code. The board is not displaying anything. Let me try LCD.zip code. But Is it enough if I just flash the code present inside this zip folder (lcd.zip)? Or any other files required? What should be the boot configuration settings?2004-08-05 12:00 AM
As you sugeested we used this file in debugging mode.
We were able to see some segments of the LCD blinking We could monitor Enable signal toggling at the LCD ( 6'th Pin). ( I think some portion of LCD has gone bad). Now in the second phase I flashed the same code. My expectation is to observe the same phenomenon on the LCD display. But I didnt see any blinking on the LCD screen which I observed in the previous experiment. Could you help me in this regard...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.